mcu link pro with mimxrt1060 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcu link pro with mimxrt1060 evk

221 Views
tomerk
Contributor I

Hello,

I am currently working with an MCU-Link Pro Debug Probe and a RT1060EVK.

My goal is to test the debug functionality of the MCU-Link Pro for a board that will be using a RT1062 and will not include the on-board debugger circuit of the EVK.

My question is, are there any modifications that need to be done to the MCU-Link Pro or RT1060EVK (Removing jumpers, breaking traces, switch configurations, etc...) for me to be able to achieve communication between the two? What I have tried so far is I have the debug probe connected to my host PC, and I am connecting the J7 port of the debug probe to the J34 port of the EVK through a 10 pin jumper. When attempting to flash in any rt1060 i get errors.

thanks

0 Kudos
1 Reply

185 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @tomerk,

There shouldn't really be any extra changes from what comes out of the box on either of these devices for them to work in conjunction. What kind of error are you facing? Is there a log or image you can show about these issues? Do you also get these errors when using different debug probes? Or only when using the MCU-Link Pro?

BR,
Edwin

0 Kudos