I am using a custom board with IMXrt1170. I have run the graphics accelerator example in SDK 2.14.0
When EW_USE_FREE_RTOS flag is enabled, example runs very well. However, when the flag is disabled, it not.
I need that example with no FreeRtos. I want GPU2D, VGLite, to use directly on bare metal without RTOS.
Hello @burhanhagi,
Unfortunately, the Embedded Wizard examples for the RT1170 uses FreeRTOS.
Nonetheless, according to i.MX RT1170 - Embedded Wizard: "[…]a few additional settings can be configured directly within the Makefile, like the usage of the FreeRTOS operating system."
Could you please take a look at the following community post: How do I choose if FreeRTOS is used or not in the PXP version of the software for RT1170? - Ask Embe...?
In case you still have some issues changing the EW_USE_FREE_RTOS=0 you could go to the .cproject and change it there.
Warm regards, Raul.