imxrt1010 usb_dev_audio_speaker_bm example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1010 usb_dev_audio_speaker_bm example

239 Views
SergioNpl
Contributor I

Hi!

Configuration Descriptor in example has the following values:

number of bytes occupied by one audio subslot - 2

number of effectively used bits from the available bits in an audio subslot - 16

Any other values not work.(for example: bSubslotSize=2 bBitResolution=8;)

There are no error messages during initialization (win10),

but playback is not going on. Some players report: "Unrecoverable playback error: Unsupported stream".

I have studied the UAC2.0 standard, but I have not found other places where it is necessary to specify the bit depth of the samples.

Can someone help me ?

0 Kudos
1 Reply

178 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @SergioNpl ,

 

Which SDK version you are using? So far the latest supports RT1010 is ver 2.14.0 , but I could not find something like bBitResolution in the latest version. Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos