iMXRT1052 EVK printer support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1052 EVK printer support

613 Views
EmbeddedTech
Contributor III

Hi,

I am currently working with iMXRT1052 EVK and we are in prototyping phase. I am looking to verify the host printer support in the SDK. I would like to connect my home printer SCX 3400 Samsung printer to the EVK. Should I use the USB B to USB micro B cable to connect the printer to the USB device connector in the EVK? Also is there any procedure to install the driver to the host?

EmbeddedTech_0-1627630579038.jpeg

Thanks.

0 Kudos
3 Replies

566 Views
EmbeddedTech
Contributor III

Hi,

Does the current sample code for host printer support printers with PCL? If I want to use a printer with SPL printing language, is it possible to implement it?

Thanks.

 

 

0 Kudos

603 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @EmbeddedTech ,

Yes, you can use this cable to connect EVK and printer. There is USB host printer examples in RT1060 SDK. But there isn't any guide to install printer driver. You have to add printer drive code into project source code.

 

Regards,

Jing

0 Kudos

587 Views
EmbeddedTech
Contributor III

Hi Jing,

I will try with the printer and get back to you if I need any help on this.

Thanks.

0 Kudos