i.MXRT1021 ETM trace port size?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1021 ETM trace port size?

1,132 Views
chris_eyre
Contributor I

What is the supported ETM trace port size on the RT1021? The 1020 reference manual suggests that TRACEDATA can be 1, 2, or 4 bits and 4-bit mode is recommended (see 7.2.2.2 CoreSight trace port interface). However, this seems to conflict with the actual behavior of the device. With a debug connection to the 1021 evaluation kit. I observed that the ARM TPIU Supported Port Size register is fixed to 1 (0xE0040000=0x00000001). If my understanding is correct, this register indicates that only PORT_SIZE=1 is supported by the device and this cannot be changed. My evaluation kit has been modified to support ETM trace and I was able to verify that 1-bit ETM trace is working, but not 2-bit or 4-bit mode.

We are evaluating the 1021 as a possible migration from the K24. With the k24 we are using 4-bit TRACEDATA  mode and this seems to meet our needs. On the k24 I confirmed that the Supported Port size register indicates 4-bit mode is supported. ETM trace is important for our applications so I am concerned with the apparent limit of 1-bit ETM Trace and at this point it is unclear whether this will cause some kind of trace data bottleneck. 

Labels (1)
0 Kudos
3 Replies

872 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Chris Eyre,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I've also checked the value of TPIU_SSPSR (Supported Parallel Port Size Register) for confirmation, it seems that the RT1020 only support the 1-bit trace port, however, I still need to confirm it with the AE team and inform you if I get some replies from them.

pastedImage_2.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

872 Views
Aubineau_FAE
NXP Employee
NXP Employee

Hi,

Strange, in the SDK you clearly see you have 4 TRACE pin:

Search "trace" (6 hits in 1 file)
 C:\Users\nxa22167\AppData\Local\Temp\1\Temp1_SDK_2.6.1_EVK-MIMXRT1020.zip\devices\MIMXRT1021\drivers\fsl_iomuxc.h (6 hits)
 Line 466: #define IOMUXC_GPIO_AD_B0_10_ARM_CM7_TRACE_CLK 0x401F80E4U, 0x6U, 0, 0, 0x401F8258U
 Line 474: #define IOMUXC_GPIO_AD_B0_11_ARM_CM7_TRACE_SWO 0x401F80E8U, 0x6U, 0, 0, 0x401F825CU
 Line 482: #define IOMUXC_GPIO_AD_B0_12_ARM_CM7_TRACE00 0x401F80ECU, 0x6U, 0, 0, 0x401F8260U
 Line 491: #define IOMUXC_GPIO_AD_B0_13_ARM_CM7_TRACE01 0x401F80F0U, 0x6U, 0, 0, 0x401F8264U
 Line 500: #define IOMUXC_GPIO_AD_B0_14_ARM_CM7_TRACE02 0x401F80F4U, 0x6U, 0, 0, 0x401F8268U
 Line 509: #define IOMUXC_GPIO_AD_B0_15_ARM_CM7_TRACE03 0x401F80F8U, 0x6U, 0, 0, 0x401F826CU

In the i.MXRT1050 it is the same and the app note 12437 descritbe it page :

https://www.nxp.com/docs/en/application-note/AN12437.pdf 

BR

V.

0 Kudos

872 Views
jeremyzhou
NXP Employee
NXP Employee

Hi vincent.aubineau,

Thanks for your reply,
I think the post can answer your inquiry.

RT1052/RT1061 trace port width 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos