i.MX 1015 FlexSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 1015 FlexSPI

785 Views
kensu
Contributor V

Hi,

There are two FlexSPI channel on i.MX1015,

My boot image is execute on QSPI Nor Flash(use FLEXSPI_A Flash A1), in this condition,

I want to program another QSPI flash(Flash B1) in my application which is running on Flash A1.

pastedImage_1.png

Is it possible?

Thanks

Ken

Labels (1)
Tags (1)
4 Replies

630 Views
armandc_
Contributor III

Hi Ken Su,

I recommend you to read AN12564.

Armand

0 Kudos

630 Views
kensu
Contributor V

Hi Armand

I had check the AN12564, it's good information for me, thanks.

And I think I will choose "Dedicated RWW Flash Device" solution.

I have some question.

Q1: What sample code can I reference if I use dedicated RWW Flash Device

I download "evkmimxrt1015_flexspi_nor_polling_transfer".

I am a little confused.

Q2: Does this sample code execute boot image on external QSPI Flash and also write data to same QSPI Flash?

pastedImage_1.png

Regards

Ken

0 Kudos

630 Views
armandc_
Contributor III

Hi Ken,

On our system we used a different approach, we are running the code that modifies the flash from RAM with IRQ locked. Therefore I cannot give advice on the code given in the application note because I never used it. But I'm sure someone from NXP can help you with that.

Regards,
Armand

0 Kudos

630 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Ken Su,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
1) Is it possible?
-- Yes, it's possible.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------