hard fault set, shows Imprecise data bus error after running for several hours.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

hard fault set, shows Imprecise data bus error after running for several hours.

891件の閲覧回数
niz
Contributor III

When we are doing a durability test on the CAN send and receive, we had the following hard fault after running the software for several hours: 

niz_0-1673621253054.png

The Imprecise data bus error bit is set in the BFSR register. 

The fault happened randomly after the software has been running for several hours. 

We are using NXP MXRT1064 

Any clue or suggestion would be appreciated. 

 

Thanks a lot for your help. 

 

Ni 

 

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

557件の閲覧回数
youngSheldon
Contributor II

Hello,

I'm having a similar issue, the only difference is that I am starting/stopping a PIT triggered by a rising and falling edge interrupt respectively. Sometimes the code runs fine, sometimes it is slopy and sometimes throws a FAULT.

I tried setting priorities for the 2 interrupts with no effect. I used other pins with no effect. Seems to be a configuration matter, but I can;t put my finger on it. Sampe code below.

BOARD_ConfigMPU();
BOARD_InitBootPins();
BOARD_InitBootClocks();
NVIC_SetPriority(GPIO1_Combined_0_15_IRQn, 0U);//this doesn't solve the issue, although increases consistency
NVIC_SetPriority(GPIO2_Combined_0_15_IRQn, 1U);//this doesn't solve the issue, although increases consistency
BOARD_InitBootPeripherals();

youngSheldon_0-1703500874359.png

 

let it flow
0 件の賞賛
返信

888件の閲覧回数
niz
Contributor III

Some more background information, this is the custom board that we are building. 

 

0 件の賞賛
返信