booting related imxrt117x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

booting related imxrt117x

1,696 Views
aravindhg
Contributor II

hi sir 

we used QSPI  interface based fused booting process. we used evk board same layout for boot interface  .we are using external flash .
wire acknowledge fault . its not working. Help us out.

Do i have to do any thing else?

0 Kudos
Reply
5 Replies

1,662 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be suppurating your case, I have some questions.

What kind of memory are you using?
Did you achieve the flash in the past? or is it the first time that you are testing your new PCB?
Could you tell me about the fuses did you burn?
Could you tell me about the boot config and boot mode?
What interface are you using to communicate SWD or JTAG?
What kind of debugger are you using?
What kind of IDE or tool are you using to flash?
Do you think the communication with external memory is ok? 

Could you try to use secure provisioning to test de communication? you must need the board in serial downloader to communicate with the tool.

Pavel_Hernandez_0-1688077802283.png

In the point 1 you could test your memory communication.
In point 2 you could read the fuses.

Best regards,
Pavel

0 Kudos
Reply

1,620 Views
aravindhg
Contributor II

 secure provisioning test results 

0 Kudos
Reply

1,476 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I sent you a mail with the internal case, could you review this in your inbox?

Best regards,
Pavel

0 Kudos
Reply

1,630 Views
aravindhg
Contributor II
Hi,
we are using the following :
1.QSPI based winbond external flash.
2.Yes, but we are facing issues in the newly designed card which is almost similar to our old card.
3.fuses burned as per internal boot mode.
4.boot config and boot mode are internal boot mode.
5. we are using the SWD
6.MCUxpresso link debugger
7. we are using the latest version of MCUxpresso 11.6
8.communication with external flash is not sure, controller is unable to load the code into QSPI flash
regards,
Aravindh
0 Kudos
Reply

1,596 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, could you please open an internal case? and tag [write] my name?

Best regards,
Pavel

0 Kudos
Reply