Zephyr MIMXRT1050-EVK Ethernet support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Zephyr MIMXRT1050-EVK Ethernet support

Jump to solution
1,432 Views
jm2
Contributor I

Hi,

It seems that the MCUX Ethernet driver has not been enabled in the port of the mimxrt1050-evk to the Zephyr OS. I see that there is an active issue (#8900) in the zephyr project github to add this, can anyone tell me when we might expect it?

Thanks. 

0 Kudos
1 Solution
1,235 Views
maureen
NXP Employee
NXP Employee

Hi Jeremy,

We are starting to work on it now, so it will be available in the next release (1.14). You can subscribe to the GitHub issue to get an automatic notification when support gets merged into the upstream master branch.

Maureen

View solution in original post

0 Kudos
1 Reply
1,236 Views
maureen
NXP Employee
NXP Employee

Hi Jeremy,

We are starting to work on it now, so it will be available in the next release (1.14). You can subscribe to the GitHub issue to get an automatic notification when support gets merged into the upstream master branch.

Maureen

0 Kudos