Dear Sir/ Ma'am
We are looking for Media Processor having ultra low power features and with following interface:
1. 24 bit RGB Camera input with HSYNC,VSYNC,DE
2. 8 bit Parallel Video Input
3. 24 bit Video Output for OLED
4. Analog Video output for 7" LCD
5. SD Card support upto 256GB
6. Keypad Interface
7. Power Consumption should be Less than 1.2W with 1 video input and 1 video output and Keypad running.
Hi Subham
first one can look i.MX comparison table
https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf
There are no much i.MX processors with several parallel camera inputs, probably
better suitable option would be i.MX6S:
AN4715, i.MX 6Solo Power Consumption Measurement
https://www.nxp.com/docs/en/application-note/AN4715.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------