VDD_USB_3V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDD_USB_3V

492 Views
akkustyk
Contributor I

Hi All

I checked VDD_USB_3V on the evaluation kit, 

On one kit it is 2.5V on the other 2.6V,

Is this ok? Why it's not 3.0V?

Best

0 Kudos
1 Reply

451 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I measured the I.mxrt1050 EVKB for it. And find the voltage is 2.62v. Depends on the RM(The output of the regulator can be programmed in 25 mV steps, from 2.625V to 3.4 V .) . So it it ok. Hope it help you. Have a nice day.

Best regards

0 Kudos