Spansion (Cypress) EVK Hyper Flash driver support for smaller memories of the same family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spansion (Cypress) EVK Hyper Flash driver support for smaller memories of the same family

962 Views
diogocacador
Contributor III

Hello,

Quick question in relation to supported Hyper Flash ICs for the i.MX RT1050 family:

Does the driver provided (MIMXRT1050-EVK_S26KS512S.cfx) in the SDK support other Cypress(Spansion) memory sizes of the same family? (EVK uses 512Mb but there are also 256 and 128 Mb version out there)

Best regards,

Diogo

Labels (1)
0 Kudos
Reply
1 Reply

822 Views
igorpadykov
NXP Employee
NXP Employee

Hi Diogo

for other supported parts one can look at AN12107 How to Enable Boot from
HyperFlash and SD Card sect.4. HyperFlash support list
https://www.nxp.com/docs/en/application-note/AN12107.pdf


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply