Secure provisioning of RT1021 by a third party?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure provisioning of RT1021 by a third party?

135 Views
rshipman
Contributor V

Is there a way of provisioning an RT1021 so that it can be done by a third party without compromising the software IP?

I've come to the conclusion that the answer is no, because you need a trusted person to first burn the fuses/keys etc into the RT1021 and any secure code into flash.

I was just wondering if anyone had some thoughts on this?

Ideally we would like to outsource the manufacturing of the entire product, but I don't think we can because the RT1021 needs provisioning securely.

0 Kudos
1 Reply

72 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @rshipman ,

 

Maybe you can connect RT with a SE like SE050E2 and use the keys inside the SE instead, you know , the keys in SE are trust provisioned out of factory by NXP. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos