In order to register users in bulk, I want to register users with photos.
1. Can I register with only RGB image in the door access (heavy) app type?
2. Can the feature created in the user_id app type be used in other app type?
3. Is there any viznas_facereg_manager_app windows version? --> In particular, oasis_lite win32 version is required?
Solved! Go to Solution.
Hi,
Thanks for your reply.
1. Is my scenario applicable?
-- Yes, I think is possible.
2. Should I start OASIS with OASIS_IMG_TYPE_RGB_SINGLE(init param) to register user with only RGB image? or Is it possible to regiter user only RGB image in OASIS_IMG_TYPE_RGB_IR_DUAL (door access)? How can I do it?
-- When app type is APP_TYPE_USERID, then only RGB camera will be captured to s_FaceRecBuf area.
3. In demo, when changing app type, database is delete. Can I use it in differenct app types without deleting database?
-- It's available, however, it needs the customer to do secondary development.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
moved to other reply
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1. Can I register with only RGB image in the door access (heavy) app type?
-- Yes.
2. Can the feature created in the user_id app type be used in other app types?
-- Actually, I'm not very clear with the question, please explain it in detail again.
3. Is there any viznas_facereg_manager_app windows version? --> In particular, oasis_lite win32 version is required?
-- No, I'm afraid that it doesn't exist.
Hope it helps.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Below is my scenario
- Remote application send user information (user name & raw image data) through the communication channel.
- Device recognizes the face from raw image data and registers the user.
- Remote application repeats the previous task for all users.
My problem is...
In SLN_VIZNAS demo, OASIS_run_extend function requires RGB & IR image. When I passed RGB Image(which is passed from remote) & NULL IR image to the function. The function returns an error in door access. But on userid app type, The function success with ok message.
My question is...
1. Is my scenario applicable?
2. Should I start OASIS with OASIS_IMG_TYPE_RGB_SINGLE(init param) to register user with only RGB image?
3. or Is it possible to regiter user only RGB image in OASIS_IMG_TYPE_RGB_IR_DUAL (door access)? How can I do it?
4. In demo, when changing app type, database is delete. Can I use it in differenct app types without deleting database?
Hi,
Thanks for your reply.
1. Is my scenario applicable?
-- Yes, I think is possible.
2. Should I start OASIS with OASIS_IMG_TYPE_RGB_SINGLE(init param) to register user with only RGB image? or Is it possible to regiter user only RGB image in OASIS_IMG_TYPE_RGB_IR_DUAL (door access)? How can I do it?
-- When app type is APP_TYPE_USERID, then only RGB camera will be captured to s_FaceRecBuf area.
3. In demo, when changing app type, database is delete. Can I use it in differenct app types without deleting database?
-- It's available, however, it needs the customer to do secondary development.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------