SEMC Serial NAND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SEMC Serial NAND

806 次查看
Ankush_9881
Contributor II

Hello All,

 I am working with iMXRT1176, I have one query like, Is it possible to interface Serial SLC NAND flash via SEMC1 and boot the MCU ?

Also with above configuration , is it possible to use SDRAM and SLC NAND Flash on SEMC ?

(example: NAND Flash MX35LFxGE4AB) 

0 项奖励
2 回复数

382 次查看
maouncle
Contributor I

Can you recommand one type nand device for iMXRT1176?

0 项奖励

785 次查看
jay_heng
NXP Employee
NXP Employee

SEMC can only work with Raw NAND (ONFI 1.0), you can use FlexSPI to interface Serial (SPI) NAND (JESD216).

it is possible to use SDRAM and Raw NAND Flash on SEMC

0 项奖励