SEMC SRAM interface_Higher address A[M : 16]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SEMC SRAM interface_Higher address A[M : 16]

775 Views
ShiXiang
Contributor I

product: I.mxrt 1170 series

For the SRAM write/read in SYNC mode (ADMUX), just wonder is it possible to mask the higher address bit, A[M : 16] and UB&LB, means not to use and free up my address pin, so that I can connect them to extra GPIOs? 

My SRAM application only need A0-15. (which share together with D0-15)

Can the software call function/register support on masking or is the software/register adjustable? For masking the higher address bit, A[M : 16] and UB&LB, while using SRAM write/read in SYNC mode (ADMUX) . Thank you.

Or if we did not call the A[M : 16] and UB&LB, is it means we mask the features and free up those GPIOs? 

0 Kudos
1 Reply

762 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @ShiXiang ,

Yes, In ADMUX mode, you can take unused address pins as gpio or other function.  

 

Regards,

Jing

0 Kudos