Recovering an iMXRT1060-EVKB with USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recovering an iMXRT1060-EVKB with USB

411 Views
arseniivanov
Contributor I

Hello, I might have bricked my Evaluation kit board.

After a debug run, I can no longer find the board using the MCUXpresso IDE, it simply returns the info below when i try to debug with a build.

"""
0 available SWD Devices detected.
Connect a device and try again.
"""
I can access it and start it in Maintenance mode by holding the power, but it does not accept .bin files of the bootloader such as the "lpc4322_bl_crc.bin" as it simply returns "FAIL.txt".

I can access the board and make changes, but how can I recover it from here?

Here is the info in DEATILS.txt:

# DAPLink Firmware - see https://mbed.com/daplink
Unique ID: 0229000033f5585d00000000000000000000000097969905
HIC ID: 97969905
Auto Reset: 0
Automation allowed: 0
Overflow detection: 0
Daplink Mode: Interface
Interface Version: 0246
Bootloader Version: 0244
Git SHA: 51140ef2aa7be53bca9e15ca7ef7acef05ff6527
Local Mods: 1
USB Interfaces: MSD, CDC, HID, WebUSB
Bootloader CRC: 0xe493996b
Interface CRC: 0xf7f2f5dd
Remount count: 0

Labels (1)
0 Kudos
Reply
1 Reply

401 Views
arseniivanov
Contributor I

Problem was a faulty state on the debug chip caused by very faulty builds.
Fixed by disconnecting J9, attaching JTAG and reflashing the board with SW from the JTAG.

0 Kudos
Reply