Recommend a RT device that supports 2-channel camera input and display at same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommend a RT device that supports 2-channel camera input and display at same time

552 Views
JK_Cha
Contributor IV

Hi 

Could you please recommend a RT device that supports 2-channel camera input and display at same time?

The application is similart with 2ch-dash cam.

Regards, 

Jack

0 Kudos
1 Reply

545 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @JK_Cha ,

  May I consider you want to use two CSI at the same time?

  If yes, we recommend you one use the CSI API, another use the flexIO to simulate the CSI to connect your camera.

  Normal CSI, you can refer to the RT SDK CSI code, flexIO emulate CSI, please refer to this AN:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

https://www.nxp.com/docs/en/application-note-software/AN12686SW.zip

 

Wish it helps you!

Best Regards,

Kerry