Read & Write data to qspi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read & Write data to qspi

769 Views
venugopal_v
Contributor III

In one of the project i am using imxrt1050 mcu with qspi flash. i need to store some configuration data in to qspi  runtime ,i can see sdk example that use RAM  to do this but how can i do with flash?if any example or guide please provide

i have referred to A way to create a binary that is copied to RAM from the ROM bootloader in RT1050  i tried adding  flash api in to this  ,normal code works but coping data has some fault

Labels (1)
0 Kudos
1 Reply

685 Views
FelipeGarcia
NXP Employee
NXP Employee

This is a duplicated thread. See conversation in this thread.

0 Kudos