RT1189 evb board loopback spi fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1189 evb board loopback spi fail

317 Views
hatemahmoudi
Contributor I

I'm running the lpspi_loopback example program on an RT1189, and have wired together pins J44-8 and J44-10 (MISO & MOSI), but the masterRxData[] array is filled with zeroes and the test fails. Have I overlooked any configurations or settings?

0 Kudos
Reply
1 Reply

289 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @hatemahmoudi ,

 

Thanks for reaching out! Is there any NXP FAE following your project? Actually RT118x is NPI which is directly supported by NXP FAE team , we have no info regarding this chip so far. Please kindly contact the FAE for further support.

 

Thanks for your patience and understanding!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply