RT1176 Custom Board SDRAM Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 Custom Board SDRAM Test

301 Views
Wobaffet
Senior Contributor I

Hello,

We've a custom board with RT1176 MCU. For the SDRAM we are using EM638165BM-5IH from EtronTech which is 4M x 16-bit SDRAM. To test the SDRAM, we are using an example project from the RT1170 EVK board SDK cm7_semc example source code to initiate SDRAM. We have made the below changes for the initialization of semc for our SDRAM:

 Below, we have not changed the timing settings, only the size, port size, and DQS mode changed w.r.t original project.

 

 

status_t BOARD_InitSEMC(void)
{
    semc_config_t config;
    semc_sdram_config_t sdramconfig;
    uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

    /* Initializes the MAC configure structure to zero. */
    memset(&config, 0, sizeof(semc_config_t));
    memset(&sdramconfig, 0, sizeof(semc_sdram_config_t));

    /* Initialize SEMC. */
    SEMC_GetDefaultConfig(&config);
    config.dqsMode = kSEMC_Loopbackinternal; /* For more accurate timing. */
    SEMC_Init(SEMC, &config);

    /* Configure SDRAM. */
    sdramconfig.csxPinMux           = kSEMC_MUXCSX0;
    sdramconfig.address             = 0x80000000;
    sdramconfig.memsize_kbytes      = 2 * 4 * 1024;       /* 64MB = 2*32*1024*1KBytes*/
    sdramconfig.portSize            = kSEMC_PortSize16Bit; /*two 16-bit SDRAMs make up 32-bit portsize*/
    sdramconfig.burstLen            = kSEMC_Sdram_BurstLen8;
    sdramconfig.columnAddrBitNum    = kSEMC_SdramColunm_9bit;
    sdramconfig.casLatency          = kSEMC_LatencyThree;
    sdramconfig.tPrecharge2Act_Ns   = 15; /* tRP 15ns */
    sdramconfig.tAct2ReadWrite_Ns   = 15; /* tRCD 15ns */
    sdramconfig.tRefreshRecovery_Ns = 70; /* Use the maximum of the (Trfc , Txsr). */
    sdramconfig.tWriteRecovery_Ns   = 2;  /* tWR 2ns */
    sdramconfig.tCkeOff_Ns =
        42; /* The minimum cycle of SDRAM CLK off state. CKE is off in self refresh at a minimum period tRAS.*/
    sdramconfig.tAct2Prechage_Ns       = 40; /* tRAS 40ns */
    sdramconfig.tSelfRefRecovery_Ns    = 70;
    sdramconfig.tRefresh2Refresh_Ns    = 60;
    sdramconfig.tAct2Act_Ns            = 2; /* tRC/tRDD 2ns */
    sdramconfig.tPrescalePeriod_Ns     = 160 * (1000000000 / clockFrq);
    sdramconfig.refreshPeriod_nsPerRow = 8 * 1000000 / 8192; /* 64ms/8192 */
    sdramconfig.refreshUrgThreshold    = sdramconfig.refreshPeriod_nsPerRow;
    sdramconfig.refreshBurstLen        = 1;
    sdramconfig.delayChain             = 6; /* For all tempeatures. */

    return SEMC_ConfigureSDRAM(SEMC, kSEMC_SDRAM_CS0, &sdramconfig, clockFrq);
}

 

 

 As for our questions, 

 1- When we run the code, read-write for 32 bits at both 59MHz and 198Mhz fails, after some time it overwrites on the same area on the SDRAM when storing indexes, but when we store a single value for each index, test successes. Why is that?

 

 

sdram_writeBuffer[index] = index; //original code, storing index
sdram_writeBuffer[index] = 5; //successing code, storing single value

void SEMC_SDRAMReadWrite32Bit(void)
{
    uint32_t index;
    uint32_t datalen = SEMC_EXAMPLE_DATALEN;
    uint32_t *sdram  = (uint32_t *)EXAMPLE_SEMC_START_ADDRESS; /* SDRAM start address. */
    bool result      = true;

  //  PRINTF("\r\n SEMC SDRAM Memory 32 bit Write Start, Start Address 0x%x, Data Length %d !\r\n", sdram, datalen);
    /* Prepare data and write to SDRAM. */
    for (index = 0; index < datalen; index++)
    {
        sdram_writeBuffer[index] = 5;
        sdram[index]             = sdram_writeBuffer[index];
        if (sdram_writeBuffer[index] != sdram[index])
        {
            result = false;
            break;
        }
    }

   // PRINTF("\r\n SEMC SDRAM Read 32 bit Data Start, Start Address 0x%x, Data Length %d !\r\n", sdram, datalen);

#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
    DCACHE_InvalidateByRange(EXAMPLE_SEMC_START_ADDRESS, 4U * SEMC_EXAMPLE_DATALEN);
#endif

    /* Read data from the SDRAM. */
    for (index = 0; index < datalen; index++)
    {
        sdram_readBuffer[index] = sdram[index];
    }

 //   PRINTF("\r\n SEMC SDRAM 32 bit Data Write and Read Compare Start!\r\n");
    /* Compare the two buffers. */
    while (datalen--)
    {
        if (sdram_writeBuffer[datalen] != sdram_readBuffer[datalen])
        {
            result = false;
            break;
        }
    }

    if (!result)
    {
        PRINTF("\r\n SEMC SDRAM 32 bit Data Write and Read Compare Failed!\r\n");
    }
    else
    {
        PRINTF("\r\n SEMC SDRAM 32 bit Data Write and Read Compare Succeed!\r\n");
    }
}

 

 

Wobaffet_0-1692789313646.png

Wobaffet_1-1692789389996.png

 

 

2- Why does dqs.Mode affects our outcome even though our layout is the same as EVK, On EVK dqs.Mode is config.dqsMode = kSEMC_Loopbackdqspad; but when we set dqs.Mode to  kSEMC_Loopbackdqspad example project read-write test fails even for the single value case.

3- For the timing parameters, how should we adjust them, on the datasheet of EM638165BM-5IH, things are not clear enough so that we can use the values given on the datasheet. Can you give any advice? 

Thank you in advance!

Best Regards,

0 Kudos
1 Reply

279 Views
Wobaffet
Senior Contributor I

We were using 8M SDRAM with 4 banks, each bank is 2M, 16-bit SDRAM, and 12-bit Row size, so we changed the column size to 8 bits. Eventually, worked well with some timing parameter changes but my question regarding the dqs mode stands still.

Thank you in advance! 

0 Kudos