RT1064 / Enable all 1MB SRAM for Zephyr [Resize OCRAM]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 / Enable all 1MB SRAM for Zephyr [Resize OCRAM]

784 Views
rpk
Contributor II

Hello,

By default the Zephyr devicetree for MIMXRT1064-EVK gives access to only 768KB of SRAM (OCRAM). My application needs access to the full 1MB of SRAM available on-chip. I would like to disable ITCM/DTCM and have one contiguous OCRAM memory block from 0x20200000 to 0x202fffff.

The device tree has been modiffied with the following overlay:

 

/ {

	soc {
		flexram: flexram@400b0000 {
			itcm: itcm@0 {
				status = "disabled";
			};
			dtcm: dtcm@20000000 {
				status = "disabled";
			};
			ocram: ocram@20200000 {
				status = "okay";
				reg = < 0x20200000 0x100000 >;
			};
		};
	};
};

/ {
	chosen {
		zephyr,sram = &ocram;
	};
};

 

 

Result of compilation (1MB of SRAM seemingly available):

 

[100%] Linking C executable zephyr.elf
Memory region         Used Size  Region Size  %age Used
           SDRAM:          0 GB        32 MB      0.00%
           FLASH:      912064 B         4 MB     21.75%
            SRAM:      418773 B         1 MB     39.94%
        IDT_LIST:          0 GB         2 KB      0.00%
Generating files from zephyr.elf for board: mimxrt1064_evk
[100%] Built target zephyr_final

 

This device tree change does not automatically change the ITCM/DTCM/OCRAM memory allocations. To do so I have added the following code to Reset.S:

 

/* Configure RT1064 for 1MB OCRAM  */
cpsid   i                   // Mask interrupts|
LDR     R0, =0x400ac044     // IOMUXC_GPR_GPR17
LDR     R1, =0x55555555     //
STR     R1, [R0]            // [IOMUXC_GPR_GPR17] := 0x55555555 (All banks OCRAM)
LDR     R0, =0x400ac040     // IOMUXC_GPR_GPR16
LDR     R1, =0x04           //
LDR     R3, [R0]            // R3 := [IOMUXC_GPR_GPR16] 
BFC     R3, #0,#2           // Clear bits D1 & D0 of R3 to disable DTCM and ITCM 
ORR     R2, R1,R3           // R2 := R3 OR R1 (0x04 == use FLEXRAM_BANK_CFG to config)
STR     R2, [R0]            // [IOMUXC_GPR_GPR16] := (use FLEXRAM_BANK_CFG to config)

LDR     R0, =0x400ac038     // IOMUXC_GPR_GPR14
LDR     R1, [R0]            // R1 := [IOMUXC_GPR_GPR14] 
BFC     R1, #16,#8          // Clear bits D23-D16 of R1 to set DTCM and ITCM sizes to 0 
STR     R1, [R0]            // [IOMUXC_GPR_GPR14] := Size of DTCM/ITCM adjusted down to 0 
cpsie   i                   // Unmask interrupts

 

 

A peek at the zephyr.lst file shows that the reset vector indeed points to __start,

 

70002000 <_vector_table>:
70002000:	88 78 25 20 0d 14 07 70 71 06 0a 70 79 14 07 70     .x% ...pq..py..p
70002010:	79 14 07 70 79 14 07 70 79 14 07 70 00 00 00 00     y..py..py..p....

 

 

where my inserted code is the first to run:

 

7007140c <__start>:
SECTION_SUBSEC_FUNC(TEXT,_reset_section,__start)


/* Configure RT1064 for 1MB OCRAM  */
cpsid   i                   // Mask interrupts|
7007140c:	b672      	cpsid	i
LDR     R0, =0x400ac044     // IOMUXC_GPR_GPR17
7007140e:	4816      	ldr	r0, [pc, #88]	; (70071468 <__start+0x5c>)
LDR     R1, =0x55555555     //
70071410:	f04f 3155 	mov.w	r1, #1431655765	; 0x55555555
STR     R1, [R0]            // [IOMUXC_GPR_GPR17] := 0x55555555 (All banks OCRAM)
70071414:	6001      	str	r1, [r0, #0]
LDR     R0, =0x400ac040     // IOMUXC_GPR_GPR16
70071416:	4815      	ldr	r0, [pc, #84]	; (7007146c <__start+0x60>)
LDR     R1, =0x04           //
70071418:	f04f 0104 	mov.w	r1, #4
LDR     R3, [R0]            // R3 := [IOMUXC_GPR_GPR16] 
7007141c:	6803      	ldr	r3, [r0, #0]
BFC     R3, #0,#2           // Clear bits D1 & D0 of R3 to disable DTCM and ITCM 
7007141e:	f36f 0301 	bfc	r3, #0, #2
ORR     R2, R1,R3           // R2 := R3 OR R1 (0x04 == use FLEXRAM_BANK_CFG to config)
70071422:	ea41 0203 	orr.w	r2, r1, r3
STR     R2, [R0]            // [IOMUXC_GPR_GPR16] := (use FLEXRAM_BANK_CFG to config)
70071426:	6002      	str	r2, [r0, #0]

LDR     R0, =0x400ac038     // IOMUXC_GPR_GPR14
70071428:	4811      	ldr	r0, [pc, #68]	; (70071470 <__start+0x64>)
LDR     R1, [R0]            // R1 := [IOMUXC_GPR_GPR14] 
7007142a:	6801      	ldr	r1, [r0, #0]
BFC     R1, #16,#8          // Clear bits D23-D16 of R1 to set DTCM and ITCM sizes to 0 
7007142c:	f36f 4117 	bfc	r1, #16, #8
STR     R1, [R0]            // [IOMUXC_GPR_GPR14] := Size of DTCM/ITCM adjusted down to 0 
70071430:	6001      	str	r1, [r0, #0]
cpsie   i                   // Unmask interrupts
70071432:	b662      	cpsie	i

 

 

When run a lot of the initial expected log is shown in console but eventually the system crashes before the boot process completes: 

 

rpk_0-1626420920710.png

If I keep the OCRAM at the default 768KB and make no changes to Reset.S then the system boots nicely w/o any problems.

Very grateful for any pointers as to what I am doing wrong here.

/Rolf

 

 

Labels (1)
0 Kudos
0 Replies