RT1064调整OCRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064调整OCRAM

5,277 Views
colinluan
Contributor III

Hi @jeremyzhou 

我想把RT1064的OCRAM调整至1MB(之前默认的配置是768KB, 128KB, 128KB),参考了相关的文档及帖子后调整步骤如下:

1、RsetISR中对FlexRAM调整

1.png

2、XIP文件中做出相应修改

2.png

3、IDE中做出调整

3.png

4、MPU中做出调整

4.png

这一步我取消了ITCM与DTCM,所以在MPU中取消了这两部分,并且后面的序号顺延,这部分的修改是否会有问题?

5、编译并且调试

5.png

 最终调整后可以正常编译,并且Jlink可以正常连接,但是每次运行到FreeRTOS创建任务时就飞掉,而用之前默认的内存映射就可以正常运行,可以帮助我分析一下吗?谢谢!

0 Kudos
10 Replies

5,272 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
建议参考此篇经验分享来完成FlexRAM重新配置:
https://www.nxpic.org.cn/module/forum/thread-619452-1-1.html
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

5,265 Views
colinluan
Contributor III

我看了下链接,有两个疑问:

1,RT1050_connect_128Kocram_128Kitcm_256Kdtcm.scp

我看文章里用的linkserver来debug的,这个文件对于Jlink来说也是一样需要的吗?

 

2,如果我想把ITCM跟DTCM调整为0,MPU该如何调整?这两段直接去掉吗?别的段需不需要跟着调整?

0 Kudos

5,244 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
感谢回复。
1) 我看文章里用的linkserver来debug的,这个文件对于Jlink来说也是一样需要的吗?
-- 是的。
2 )如果我想把ITCM跟DTCM调整为0,MPU该如何调整?这两段直接去掉吗?别的段需不需要跟着调整?
-- ITCM和DTCM就无需调整,OCRAM部分还是还是要调整的,多问一句,你为什么要把ITCM跟DTCM调整为0,因为其他客户往往是要增大它们的空间。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

5,234 Views
colinluan
Contributor III

1、脚本文件错误

设置Jlink的脚本文件是按如下的方式吗?

2.png

我把参考文档中的的脚本文件直接放了进入,但是Jlink连接的时候似乎报语法错误,根本无法解析?

1.png

 2、内存不够

我现在移植一个C++项目,目前内存比较紧张,FreeRTOS需要使用大量的Heap,又不太希望扩展SDRAM,所以希望把ITCM与DTCM都并到OCRAM来当普通内存使用。

 

0 Kudos

5,184 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
感谢回复!
我这边对evkmimxrt1064_freertos_generic工程进行了跟你一样的FlexRAM配置,基本流程就是https://www.nxpic.org.cn/module/forum/thread-619452-1-1.html

给出的,debug工程没啥问题,退出debug后,工程启动运行也是正常的。

jeremyzhou_0-1603956024502.png

 

我建议重新按照流程检查一下。

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

5,172 Views
colinluan
Contributor III

你的这个RT1064_connect_new.scp是改的链接里的scp的吗?我试了好多次一直这样,一直都不认这个脚本,而且我发现你的配置界面跟我的有些区别?

我现在已经可以正确的把OCRAM调整至1MB了,但是我发现把TCM设置成0后Jlink调试时只能下载一次代码,后面再也无法下载代码,也不能擦除,必须切换到Serial download 模式擦除后再切回来,然后再下一次代码,每次都需在两个模式切换,似乎jlink的下载算法里有使用到TCM?跟如下的问题一样:

https://www.nxpic.org.cn/module/forum/thread-620523-1-1.html

那个scp脚本是为了解决这个问题的吗?

0 Kudos

5,225 Views
eric_yp_chen
Contributor I

@colinluan 

 

我在RT1052上的經驗是您必須修改Scp 腳本, 在透過J-Link 載入RAM Code 之前就透過 Scp 修改FlexRAM Register 

 

 

BR,

Eric

0 Kudos

5,167 Views
colinluan
Contributor III

我发现把TCM设置成0后,Jlink调试时只能下载一次代码,后面再也无法下载代码,也不能擦除,必须切换到Serial download 模式擦除后再切回来,然后再下一次代码,每次都需在两个模式切换。似乎jlink的下载算法里就是通过scp配置了RAM Code加载到ITCM中,而因为我把TCM禁掉了,所以没有办法加载RAM Code,导致无法擦除及编程?

关键是我试了好多次,jlink感觉连脚本的语法都检测不过,邪门了。

0 Kudos

5,156 Views
yourchoochoo
Contributor I

烧写时,烧写算法占用ram空间为0x2000000地址,但是你在启动后将0x20000000 DTCM段设置为0,就会出现这种问题,无法在启动后再次烧写,根据我的经验可以通过下面的方式解决

 

切换非flash启动方式后,重新上电,让flash中设置flexram配置代码不运行,然后在执行烧写操作;

 

0 Kudos

5,158 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
感谢回复!
我上传了我测试过的工程和对应Scp文件,你可以参考一下。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos