RT1060 power control diagram and power up sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1060 power control diagram and power up sequence

跳至解决方案
1,353 次查看
guillaume_g
Contributor II

the reference manual and the hardware development guide are clear on how to connect power if we want to use stand by mode and 32K768 clock.

guillaume_g_0-1646214225152.png

if we didn't want to have low power mode can we simplify the power diagram as follow.

 

guillaume_g_1-1646214790653.png

 

This power diagram from my understanding should satisfy power up sequence and hardware recommendation.

could you please confirm?

0 项奖励
1 解答
1,345 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @guillaume_g ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could you please confirm?
-- Yes, the simplified power supply design is available.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,346 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @guillaume_g ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Could you please confirm?
-- Yes, the simplified power supply design is available.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,012 次查看
sas1
Contributor I
I have a question if the VDD_SOC_IN (1.2V) is provided externally instead of the internal DCDC, switched by DCDC_PSWITCH with 1ms delay.
In this case, does the externally supplied 1.2V on VDD_SOC_IN also have to have a delay of 1ms?
Or is a 1ms delay not necessary in this case?
We use the MiMXRT1062DVJ6B in B-Revision (A1 silicon)
0 项奖励
1,312 次查看
masettic
Contributor II

Hello,

same question here: custom design with i.MXRT117x and power-up sequence.

Is it fine to tie together VDD_SNVS_IN, VDD_LPSR_IN, DCDC_IN AND NVCC_XXXX ?

Thank you very much, best wishes.

 

Cesare

0 项奖励