RT1050 bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 bootloader

207 Views
dskim2
Contributor III

I want to make a bootloader for IMXRT1050EVK.
The bootloader and application are stored in hyper flash, and the application is stored at 0x6008000.

The application memory is set as shown below.

dskim2_0-1702536897223.png

 

After downloading the bootloader and application to flash, run it.
It seems that only the bootloader is running and the application is not running.
What's wrong?

The application was downloaded using the GUI Flash Tool as shown in the image below.

dskim2_0-1702537281123.png

 

 

I am uploading the source as an attachment.

VTR_WOBD4_Boot is bootloader and hello_world is application

Best Regards

 

0 Kudos
1 Reply

188 Views
mjbcswitzerland
Specialist V

Hi

An off the shelf 1050 secure boot loader solution is available at https://www.utasker.com/iMX/RT1050.html
Documentation and video guides, including security analysis at https://www.utasker.com/iMX/developers.html

Regards

Mark


For our discounted i.MX and Kinetis stock availability see https://www.utasker.com/Shop/semi.html

0 Kudos