[RT1050] WiFi timer issue in HTTP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[RT1050] WiFi timer issue in HTTP

646 Views
yen_chen
Contributor III

Hi ,All

We use the wifi and connect to AP .

We want to download  file to the http server.

After connection ,it will send write request,and then receive the request in the http server and response OK.

But when we need to read the response from server to our board ,it will send

"[w_tmr] Starting timer: 20219A60 for 800 mS
read
[w_tmr] Error: Unable to start timer"

What happen the WiFi timer ?

 

log :

[w_tmr] Starting timer: 20219A60 for 800 mS
[w_tmr] Starting timer: 20219A60 for 800 mS
[INFO] [xxx] [.httpssrv_xxx.c:874] [ACTION LOG]
GET [w_tmr] Stopping timer: 20219A60
[w_tmr] Starting timer: 20219A60 for 800 mS
/xxxxx_main.bin HTTP/1.1
Host: 192.168.1.3:8000
[w_tmr] Stopping timer: 20219A60
[w_tmr] Starting timer: 20219A60 for 800 mS


[INFO] [xxx] [.httpssrv_xxx.c:889] [w_tmr] Stopping timer: 20219A60
[w_tmr] Starting timer: 20219A60 for 800 mS
[w_tmr] Stopping timer: 20219A60
[w_tmr] Starting timer: 20219A60 for 800 mS
[w_tmr] Stopping timer: 20219A60
[w_tmr] Starting timer: 20219A60 for 800 mS
[w_tmr] Stopping timer: 20219A60
[w_tmr] Error: Unable to stop timer.
[w_tmr] Starting timer: 20219A60 for 800 mS
read
[w_tmr] Error: Unable to start timer
[w_tmr] Stopping timer: 20219A60
[w_tmr] Error: Unable to stop timer.
[w_tmr] Starting timer: 20219A60 for 800 mS

 

Thanks

Br

0 Kudos
2 Replies

617 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi  Yen:

 

This issue involves with FreeRTOS timer. Could you please let me now how to reproduce your issue on my side with RT evk board?

Thanks

0 Kudos

600 Views
yen_chen
Contributor III

Hi @danielchen

We use the wifi station mode to connect to the external http server,and set the socket setting.

After connecting to socket,send the get request to server can successfully,but it will happen problem when read response from server.

Get request is for download file , file size about 700 KB.

When we use get request for other  small file(.txt),it can read file content ,so we make sure http server is ok and it actually connect to server .

 

0 Kudos