RT1050 UUID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 UUID

727 Views
ffloree
Contributor III

Does RT1050 have UUID (instead of UID)? if it does, which registers I can get it from?

I know RT685 has it, see the UM11147 Section 4.5.5.52, but I didn't find it in RT1050 reference manual, it just mentions a 8-byte UID which can be read from OCOTP->CFG0 and OCOTP->CFG1, but I don't think it's the standard 16-byte UUID following rfc4122 https://www.rfc-editor.org/rfc/rfc4122 .

Labels (1)
0 Kudos
Reply
3 Replies

697 Views
lucas_cao
NXP Employee
NXP Employee

UUID is from the fuse 0x410 and 0x420. We can use the shadow registers to get its value.For RT1050, you can use the following code to get the UUID. 

UUID_L = *(uint32_t *)0x401f4410;

UUID_H = *(uint32_t *)0x401f4420;

 

0 Kudos
Reply

716 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @ffloree ,

 

Yes, there is a thread on similar topic, and you may refer to https://community.nxp.com/t5/i-MX-RT/Read-UID-Unique-ID-on-i-MXRT-RT1050/m-p/1202637 for details.

 

You may refer to chapter 22 in the RM for more details.

Kan_Li_0-1692172115020.png

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

707 Views
ffloree
Contributor III

@Kan_Li ,

Thank you, I've seen this ticket, it talks about the Unique ID instead of Universally Unique ID. You provided the 8-byte (reg0x410 and reg0x420) data is not the UUID either. Correct me if I'm wrong.

0 Kudos
Reply