RDDI DAP error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RDDI DAP error

1,254件の閲覧回数
bilge_kara157
Contributor II

I use  i.mx rt1020 evk board.I was donwloading example projects  smoothly to the board,but then  flash error was started to give .

Keil mdk 5.24.2

Error: Flash Download failed  -  Target DLL has been cancelled

ラベル(1)
1 返信

924件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi bilge kara,

     Please check your MIMXRT1020-EVK board back side, find the SW8, power off the board, then change it to:

     SW8_1 OFF

     SW8_2 OFF

    SW8_3 OFF

    SW8_4 ON

   Then use the USB cable connect j23, connect the debug button on the MDK, I am using the SDK code:SDK_2.5.0_EVK-MIMXRT1020\boards\evkmimxrt1020\demo_apps\led_blinky\mdk

  This is the test result:

pastedImage_1.png

  You can try it on your side.

  If you want to download to the external qspi flash, choose this item:

pastedImage_2.png

Then press the LOAD button, after the download is finished, then power off the board, change the SW8 to :

     SW8_1 OFF

     SW8_2 OFF

    SW8_3  ON

    SW8_4 OFF

  Power on the board again, you will find the on board D5 is blinking, it means it works OK.

Please try it again on your side.

If you still have question about it, please kindly let me know.
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------