PWM signal from IMXRT1050 EVK GPIO_AD_B1_06 Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM signal from IMXRT1050 EVK GPIO_AD_B1_06 Pin

953 Views
sreedevi_mohan
Contributor III

Is there any method to generate PWM signal from  IMXRT1050 EVK  GPIO_AD_B1_06  Pin?

Labels (1)
0 Kudos
Reply
2 Replies

853 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

Unfortunately, GPIO_AD_B1_06 does not have any PWM signal alternative option, you can check the muxing options of all pins in chapter 10 of Reference Manual.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

853 Views
sreedevi_mohan
Contributor III

we have created a pwm signal using GPT timer example and made a clock with required frequency. But, the frequency is changing at the time of i2c write and read. How the i2c write and read is affecting the gpt timer ?  

0 Kudos
Reply