Not able to erase the flash memory location using jlink.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to erase the flash memory location using jlink.

536 次查看
madhavaishriram
Contributor II

Hi All,

I am using MIMXRT1052xxx6B controller in project with QSPI flash memory from 0x60001000 location.

I am not able to flash on to the board using jlink. It is running last loaded image and now not accepting the new image via jlink.

madhavaishriram_0-1657083482809.png

 

Please see the terminal it is running but code is not flashing on board.

When i am trying to erase using Jlink commander then i am getting 

madhavaishriram_1-1657083546957.png

this error so please if any one is having any idea regarding this please let me know the solution for this.

 

Thanks in advance.

Thanks and Regards,

Shriram Madhavai

0 项奖励
回复
1 回复

522 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I was wondering if you can introduce your testing environment, such as the board, demo code, etc.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复