MIMXRT1176AVM8A Running hot on custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1176AVM8A Running hot on custom board

329 Views
DrJonM
Contributor II

We have a couple of custom board designs using the automotive grade RT1176.

In both designs, running our application code, CPU temperature is in the high 50s C. On the EVK, (which is running the commercial grade part) temperatures with the same code are running in the high 30s so there is around a 20C difference between our boards and the EVK. Measurement with an external temperature sensor suggests these temperatures are real.

Our design is very similar to the EVK in terms of QSPI NOR flash, SDRAM and USB but it has a DSI to LVDS bridge plus uses some analogue inputs. All analogues are within range and the device functions correctly.

I have been through our design vs refernce design and all unused pins and power supplies seem to be configured the same. We are using the internal DCDC to supply the processor 1V8 and 1V0; USB 1P8 and MIPI 1P8 are supplied from a separate 1V8 supply so we are within limit for the DCDC convertor. We are running in nominal mode (not overdrive) with CM7 enabled only at 600MHz.

Reducing clock speed brings the temperature down only slightly which suggests there is some leakage or loading somewhere.

Is there any expected difference in thermal behaviour between the automotive and commercial grade parts? Are there any specific areas we should focus on to resolve this temperature discrepancy?

 

Thanks.

0 Kudos
2 Replies

288 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @DrJonM ,

 

Have you measured the current thru the pin of DCDC_IN, VDD_LPSR_IN, VDD_SNVS_IN? Are they all within the range of spec? Please kindly clarify.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

274 Views
DrJonM
Contributor II

Hi @Kan_Li 

Thank you for your replay.Our design is quite compact and unfortunately we have not had the space to put individual supply monitoring for all the rails.

VDD_SNVS_IN is measuring 1.5mA which seems high - I will try with a more accurate DVM tomorrow to confirm.

Total draw on 3v3 supply to processor is 170mA (with LCD, DSI and SDRAM disabled) which again seems high. I will compare with EVK again tomorrow.

Thanks,

Jon

0 Kudos