Hello, the MIMXRT1160-EVK has just arrived. Before purchasing, I read the specifications which stated that the kit includes x3 CAN FD buses. Unfortunately, I can't find the pins corresponding to CAN bus anywhere. I need them to create a bridge from two CAN bus ports and to forward frames from CAN1 and send on CAN2.
Can someone help me with it?
Hi @sqwerize
Thank you very much for your patience.
Eventougth the i.MX RT1160 MCU integrates 3 CAN modules the i.MX RT1160 EVK only provides a PHY for a single CAN interface. This is CAN 3. The CAN_L and CAN_H signals can be accessed through J47.
The i.MX RT1170 integrates two CAN interfaces, just in case this could help you. If you want to use your i.MX RT1160 EVK you get CAN2 and CAN1 signals from the Arduino Headers of the EVK, but keep in mind that you will need to add a PHY for each pin.
I hope this could help you.
Diego