MIMXRT1064 Serial Loader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMXRT1064 Serial Loader

669 次查看
klinsmann_mah5
Contributor I

Hi,

I recently purchased MIMXRT1064-EVK and I realize that an additional LPC4322JET100 MCU is used.

I am designing a new board and I need a USB programming port. I do not require any other debugging tools.

Can I directly connect D+ and D- of the USB to my USB port of MIMXRT1064 instead of going through an additional MCU?

or

Can I use my UART port instead?

标签 (1)
0 项奖励
1 回复

527 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi KLINSMANN MAH,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can I use my UART port instead?
-- Yes, you can.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励