MIMXRT1024-EVK JTAG not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1024-EVK JTAG not working

Jump to solution
876 Views
larrydemuth
Contributor III

I have yet to be able to get JTAG to work when trying to program and debug the eval board.

I am using MCUXpresso IDE and a PE Multilink JTAG. I can program and debug through the USB, but not JTAG. When I try, I get the following:

larrydemuth_0-1675706508526.png

I have SWD checked, and even tried it without with the same results.

Here is the Debugger settings:

larrydemuth_1-1675706725606.png

larrydemuth_2-1675706764645.png

The PE Multilink works fine when I use it with KDS IDE and a K66 micro.

What am I missing that I cant use it with the IMXRT1024?

Labels (1)
0 Kudos
Reply
1 Solution
860 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the JTAG for debugging.

First Steps with the NXP i.MX RT1020 EVK Board | MCU on Eclipse

Best regards,
Pavel

View solution in original post

0 Kudos
Reply
2 Replies
861 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the JTAG for debugging.

First Steps with the NXP i.MX RT1020 EVK Board | MCU on Eclipse

Best regards,
Pavel

0 Kudos
Reply
850 Views
larrydemuth
Contributor III

Thanks, removing jumpers J47 - J50 worked, at least for SWD mode through the PE Micro. That's good enough I guess. Still don't know why regular JTAG doesn't.

It would be nice if the User Guide would mention that though.  

0 Kudos
Reply