LVGL 8 and VGLite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVGL 8 and VGLite

766 Views
masterboy
Contributor III

Hi,

I am working on a project that uses the LVGL graphics library (8.3.8). I am using an iMX RT1060 processor as GPU. The NXP SDK I used to bring the LVGL graphics library to life uses PXP for acceleration. The LVGL library also supports VGLite acceleration. I searched the SDK for an example use case, but didn't find one. Could I get the code to use LVGL with VGLite acceleration?
Dale I wonder how much different is PXP vs VGLite? Which is more powerful?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

753 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @masterboy,

You can find code that implements VGLite acceleration bundled with Application Notes. Namely, AN13075 (and the associated AN13075SW) and AN13778 (and the associated AN13778SW).

BR,
Edwin.

0 Kudos
Reply

711 Views
masterboy
Contributor III

I'm sorry, but I didn't specify the processor I'm using in the project. It is an iMX RT 1060/1062. Does this processor support VGLite?

0 Kudos
Reply

703 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @masterboy,

Thanks for clarifying. I'm afraid the RT1060 does not support it. Sorry for the inconvenience this may cause.

BR,
Edwin.

0 Kudos
Reply