LCDIF Clock Source Freq Settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LCDIF Clock Source Freq Settings

191 Views
SpeedyGonzalesss
Contributor III

Hello,

I am using i.MX RT1176 and MCUXpresso IDE. I want to set 60 Hz for the frame rate of LCDIF and this is related to the clock source frequency. But there are four options for clock source freq:

SpeedyGonzalesss_0-1711094275082.png

 

For three options(24 MHz), actual frame rate is 57 Hz. But i need to 60 Hz. How can set frame rate for 60 Hz?

 

Thanks,

Speedy

0 Kudos
2 Replies

125 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @SpeedyGonzalesss ,

Thanks for contacting NXP support!

You could try using the Clock Tool and configure other clock sources and division ratios. Get an approximate 60Hz result.

 

Best regards,
Gavin

0 Kudos

124 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Gavin_Jia_0-1711959920628.png

 

0 Kudos