J-Link fail to erase or program RT1062

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

J-Link fail to erase or program RT1062

1,325 Views
rory
Contributor I

Hello

I'm using MIMXRT1062-EVK to debuge official Hello Word, but it fails. Then I used Jflash to erase Flash, and the following phenomenon occurred. This phenomenon also occurred when I replaced flash on the existing project board (replace the original ISIS with another one).

Can you give me some advice? Thank you.

1606959973(1).pngZXSJWJ[FLZA0[6{[CAU~Z3Q.jpg

0 Kudos
7 Replies

1,318 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi rory,

Did you configure the SW7 in QSPI-Flash Boot mode?

jingpan_0-1606979917378.png

 

Regards,

Jing

0 Kudos

1,313 Views
rory
Contributor I

Hi Jing

I've configured the SW7 in QSPI-Flash Boot mode.I measure the voltage of Flash, and it is right.

In general, what causes this situation?

Regards,

rory

 

0 Kudos

1,307 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi rory,

What flash do you use? The flash algorithm may unable to recognize your flash. You can use NXP-MCUBootUtility tool to test whether the flash is fine.

 

Regards,

Jing

0 Kudos

1,294 Views
rory
Contributor I

Hi Jing

The MIMXRT1060-EVK use IS25WP064 FLASH ,and this is the official board.

0 Kudos

1,289 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi rory,

It's hard to say what caused this problem. Please check below items.

1. RT1060 EVK use DAP-link as on board debugger. You use your own jlink. Have you disconnect J47~J50?

2. If you didn't modify the board, please check flash algrithm setting, in right click the project->properties->MCU setting. Is the flash driver set to MIMXRT1060_SFDP_QSPI.cfx?

3. In right click the project->properties->settings->Managed Linker Script, please select link application to RAM. Then try to compile and debug. Can it work? If it can't, there should be hardware setting problem. Please check power and boot config pins.

 

Regards,

Jing

0 Kudos

1,281 Views
rory
Contributor I

Hi Jing

1.I use your own jlink. J45-j50 is connected by default and I did not change it.
Are there any requirements on this side?

2.The flash driver set to MIMXRT1060_SFDP_QSPI.cfx.

3.According to your request, but failed.I'm going to power and boot config pins.

Regards,

rory

0 Kudos

1,256 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi rory,

1. Can the on board openSDA work?

2. If you use jlink, please disconnect these jumper and try again.

 

Regards,

Jing

0 Kudos