Is there FreeRTOS, FatFS and LWIP for i.MX RT1050?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there FreeRTOS, FatFS and LWIP for i.MX RT1050?

3,207件の閲覧回数
milankolar
Contributor I

Hello.

We are using STM32F4 with FreeRTOS, FatFS and LWIP. We are thinking to use i.MX RT1050. Is there this port (FreeRTOS, FatFS and LWIP) for this device? Is there another free similar library?

Thanks. Milan Kolar

ラベル(1)
3 返答(返信)

1,621件の閲覧回数
asick
Contributor III

I'm using RT1050 EVK- i want to know how to build freeRtos application with armgcc linux host machine and copy into sd card and how to get serial console application output(Ex: Hello word).

1,621件の閲覧回数
turkersezgin
Contributor III

Maybe, there is a person who knows solution :smileyhappy:

0 件の賞賛

1,621件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Milan,

the SDK for iMXRT includes FreeRTOS with lwip and FATFS. You can build your SDK here Welcome to MCUXpresso | MCUXpresso Config Tools 

Please select SDK builder and then iMXRT


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛