Implications of using PMIC_STBY_REQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implications of using PMIC_STBY_REQ

1,016 Views
karl_fraasch
Contributor III

We are looking to use the PMIC_STBY_REQ pin of the RT1064 to signal a reset to an external watchdog circuit. Issuing the reset will result in the watchdog circuit cycling the 3.3 volts to the RT1064. For our purpose, this is no different than using any other GPIO on the chip. However, we are running low on GPIO's therefore would like to use this pin if possible. This is easy enough to test on our side but we would also like to make sure there are not any implications which may not have been clear in the reference manual.

3 Replies

927 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Karl Fraasch ,

    From the RT1064 reference manual, we can get the related PMIC_STBY_REQ pin information.

pastedImage_1.png

pastedImage_2.png

So, I think you can use this pin as the GPIO5_IO02 to control the external modules. You need to set the mux as ALT5, just make sure it is not the CCM pin function.

This pin in default is the CCM pin function:

pastedImage_3.png

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

927 Views
karl_fraasch
Contributor III

Thank you Kerry, that helps!

0 Kudos

927 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Karl Fraasch,

  You are welcome!

   If your question is solved, please help me to mark the correct answer, just to close this question.

   If you have any question in the future, welcome to create the new question post.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos