IMXRT10** DCDC_OUT accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT10** DCDC_OUT accuracy

Jump to solution
760 Views
gavin5342
Contributor III

I can't see the accuracy spec for the DCDC converter on IMXRT10**.  The reason for asking is that the datasheet specifies, for VDD_SOC min 1.15V for normal operation and 1.25V for overdrive.

I have seen some SDK examples set DCDC_OUT to 1.25V for overdrive configuration and others set DCDC_OUT to 1.275V for overdrive.

0 Kudos
1 Solution
680 Views
lucas_cao
NXP Employee
NXP Employee

1.275V is the correct voltage, the 1.25V setting in SDK code should be updated.

View solution in original post

4 Replies
681 Views
lucas_cao
NXP Employee
NXP Employee

1.275V is the correct voltage, the 1.25V setting in SDK code should be updated.

675 Views
gavin5342
Contributor III

Thanks very much! That makes most sense to me too.

0 Kudos
682 Views
gavin5342
Contributor III

I am interested in the answer for RT1050 series and RT1010 series.  For both of these devices the range is 1.15 - 1.3V as you show here.

0 Kudos
748 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @gavin5342 

I hope you are doing great! 

To give you a better response :  could you specify in which part number and related SDK did you saw those parameters and  DCDC output settings?

For example, according to the RT1060 DS, the VDD_SOC_IN tolerates up to 1.3v

diego_charles_0-1693590548139.png

All the best, 

Diego

 

0 Kudos