IMXRT10** DCDC_OUT accuracy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT10** DCDC_OUT accuracy

ソリューションへジャンプ
842件の閲覧回数
gavin5342
Contributor III

I can't see the accuracy spec for the DCDC converter on IMXRT10**.  The reason for asking is that the datasheet specifies, for VDD_SOC min 1.15V for normal operation and 1.25V for overdrive.

I have seen some SDK examples set DCDC_OUT to 1.25V for overdrive configuration and others set DCDC_OUT to 1.275V for overdrive.

0 件の賞賛
返信
1 解決策
762件の閲覧回数
lucas_cao
NXP Employee
NXP Employee

1.275V is the correct voltage, the 1.25V setting in SDK code should be updated.

元の投稿で解決策を見る

4 返答(返信)
763件の閲覧回数
lucas_cao
NXP Employee
NXP Employee

1.275V is the correct voltage, the 1.25V setting in SDK code should be updated.

757件の閲覧回数
gavin5342
Contributor III

Thanks very much! That makes most sense to me too.

0 件の賞賛
返信
764件の閲覧回数
gavin5342
Contributor III

I am interested in the answer for RT1050 series and RT1010 series.  For both of these devices the range is 1.15 - 1.3V as you show here.

0 件の賞賛
返信
830件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @gavin5342 

I hope you are doing great! 

To give you a better response :  could you specify in which part number and related SDK did you saw those parameters and  DCDC output settings?

For example, according to the RT1060 DS, the VDD_SOC_IN tolerates up to 1.3v

diego_charles_0-1693590548139.png

All the best, 

Diego

 

0 件の賞賛
返信