IMXRT 1052 Storage Temperature Range

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT 1052 Storage Temperature Range

跳至解决方案
732 次查看
omerkaanbasakin
Contributor IV

Hello,

We are using i.MX RT1052. As far as we can see in the datasheet, the minimum storage temperature is -40°C. Has the test been done at -55°C? Is there information that can be given for -55°C?

Thanks in advance.

标签 (1)
0 项奖励
回复
1 解答
715 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.

Sorry for the inconvenience.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

在原帖中查看解决方案

0 项奖励
回复
1 回复
716 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.

Sorry for the inconvenience.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 项奖励
回复