IMXRT 1052 Storage Temperature Range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT 1052 Storage Temperature Range

Jump to solution
648 Views
omerkaanbasakin
Contributor IV

Hello,

We are using i.MX RT1052. As far as we can see in the datasheet, the minimum storage temperature is -40°C. Has the test been done at -55°C? Is there information that can be given for -55°C?

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Solution
631 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.

Sorry for the inconvenience.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

View solution in original post

0 Kudos
Reply
1 Reply
632 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

As mentioned in the datasheet stress beyond the maximum ratings may cause permanent damage to the device. Unfortunately, we do not have data at -55° as we cannot guarantee functional operation with ratings that are out of spec.

Sorry for the inconvenience.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply