How can I.MXRT117x MCU use IW612 play as WiFi AP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I.MXRT117x MCU use IW612 play as WiFi AP mode

545 Views
Sean14
Contributor I

Hi

 

We need to use IW612 play as WiFi AP mode, But the Host is I.MX RT 117x MCU.

However when we browse the MCUXpresso SDK, we can’t find any example project to control the IW612 as AP mode, can NXP add this WiFi AP mode function in MCUXpresso SDK? Or provide this kind sample to user? So that we could modify it into our product.

 

 

Thanks,

Sean

0 Kudos
Reply
4 Replies

523 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Please install the MCUXpresso SDK from the SDK Builder or GitHub.

Once you import the SDK into the IDE, please import the wifi_cli_cm7 or wifi_wpa_supplicant_cm7.

I recommend you to take a look to UM11442, this document is available in your SDK documentation SDK_2_15_100_MIMXRT1170-EVKB\docs\wireless. And please refer to section 3.1.5.7 Start Soft AP.

I also recommend you to take a look ot the

An example to create an AP could be:

 

#wlan-add abd ssid TEST ip:192.168.10.1,192.168.10.1,255.255.255.0 role uap wpa2 psk 12345678

 

#wlan-start-network abd

 

Regards,
Daniel.

0 Kudos
Reply

465 Views
Sean14
Contributor I

Hi Daniel,

 

Thank you for your reply,

Referring to the documentation from NXP, it seems the SDK only supports a maximum channel width of 40MHz. Could the 117x series support 80MHz?

And could NXP provide an example for 80MHz bandwidth in AP mode?

 

0 Kudos
Reply

439 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

I didn’t find any reference to 80MHz bandwidth in the documentation nor SDK in the RT family.

 

Regards,

Daniel.

0 Kudos
Reply

330 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @Sean14,

To let you know that there is a note in UM11442 that states:
NOTE: 88W8987 supports 11ac 80MHz support

Regards,

Daniel.

0 Kudos
Reply