The i.MX RT 1064 does not have the FTM found in the K22 series.
It appears that the TMR (quad timers) can perform a similar function to the FTM compare/output function.
Do I understand the TMR function correctly?
Hi Keith Smith,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Do I understand the TMR function correctly?
-- Yes, you're right.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I'm looking in the 2.6.1 iMX 1064 SDK. I found the QTMR driver, fls_qtmr.<c,h> and pwm examples, but nothing related to compare/output.
I have a suggestion. As someone upgrading from K22 to iMX, I would like to see, and I think others would too, an example of using the QTMR in the same manner as FTM compare/output. Perhaps an Appnote, as SDKs are slow to update.
This link is an example of issues upgrading to iMX from K22, looking for similar examples. https://community.nxp.com/message/1146859
Hi Keith Smith ,
Thanks for your suggestion and I'll report the suggestion in the next period of SDK field trial.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------