Does the i.MX RT1160 MIPI-CSI2 support grayscale and RAW image sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the i.MX RT1160 MIPI-CSI2 support grayscale and RAW image sensor?

Jump to solution
1,046 Views
Mc2023
Contributor IV

Hello All,

In the NXP Community forum, there are several post mentioning that the RT1170  MIPI-CSI2 can't support the raw data due to a bug.

Does the i.MX RT1160 MIPI-CSI2 support grayscale and RAW image sensor?

Best regards,

 

 

0 Kudos
1 Solution
853 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Mc2023 ,

  It is caused by the RT11XX IP, VIDE_MUX have limit which will cause the raw support issues.

 RT1170 rew RM already list the support data types:

kerryzhou_0-1691125221060.png

kerryzhou_1-1691125230064.png

RT1160 is the same.

The workaround: Use an ISP convert chip, eg, AP1302, convert the raw to MIPI CSI interface, then connect to RT1170 MIPI CSI. This is working, but it might be considered by you since this implies adding a component to your solution.
Other option is using i.MX processors with MIPI-CSI2 that can support raw type.

 

Wish it helps you!

If you have the new issues, welcome to create the new case.

Best Regards,

Kerry

 

 

 

View solution in original post

0 Kudos
6 Replies
1,028 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Mc2023 ,

  RT1160 and RT1170 is the same situation, MIPI-CSI cant support  the raw data, and no workaround now.

  If customer want to use the raw data method, they can use the parallel CSI interface instead of the mipi-csi.

https://community.nxp.com/t5/i-MX-RT/Does-the-i-MX-RT1160-MIPI-CSI2-support-grayscale-and-RAW-image/...

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
924 Views
Mc2023
Contributor IV

Hi @kerryzhou ,

Is it mentioned in an official document that MIPI-CSI does not support raw data?

Best regards,

 

0 Kudos
917 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Mc2023 ,

  Yes, new RM version will delete the raw support in the MIPI CSI.

   Sorry for the inconvenience we bring you.

   

Best Regards,

Kerry

0 Kudos
904 Views
Mc2023
Contributor IV

Hi @kerryzhou ,

Thanks for your feedback!

Now we are in an embarrassment!!!

Could you reply to the following questions:

1) What fault is it that MIPI-CSI does not do gray-scale?

2) Is it the fault of the sensor?

3) Or the processor?

4) If the processor: can we switch to another processor?

0 Kudos
854 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Mc2023 ,

  It is caused by the RT11XX IP, VIDE_MUX have limit which will cause the raw support issues.

 RT1170 rew RM already list the support data types:

kerryzhou_0-1691125221060.png

kerryzhou_1-1691125230064.png

RT1160 is the same.

The workaround: Use an ISP convert chip, eg, AP1302, convert the raw to MIPI CSI interface, then connect to RT1170 MIPI CSI. This is working, but it might be considered by you since this implies adding a component to your solution.
Other option is using i.MX processors with MIPI-CSI2 that can support raw type.

 

Wish it helps you!

If you have the new issues, welcome to create the new case.

Best Regards,

Kerry

 

 

 

0 Kudos
1,013 Views
Mc2023
Contributor IV

Hi @kerryzhou,

Thanks for your feedback!

Best regards,

0 Kudos