Documentation on using external debugger for MIMXRT1020 EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Documentation on using external debugger for MIMXRT1020 EVK?

751 Views
estacey
Contributor III

Is there documentation available for bypassing the onboard debugger on the MIMXRT1020 EVK board?  My processor won't connect just by removing jumpers I've read about in the community here and would like to be sure I'm trying everything correctly.

Thanks,

Ellen

Labels (1)
0 Kudos
1 Reply

679 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello  Ellen Stacey ,

  It's very simple to use the external debugger in MIMXRT1021-EVK board.

  You just need to remove J27 and J28, then add your own debugger, eg JLINK to the j16 jtag interface.

 pastedImage_1.png

50.jpg

pastedImage_3.png

You can find after use the external JLINK, I can find the ARM core, it means the external debugger works now.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos