Hi NXP,
In evkmimxrt1060_tensorflow_lite_kws, the example uses stereo audio to predict. Because there is only 1 mic on board (right channel), so the left channel's value is 0.
I want to change config from Stereo to Mono. I had changed
From
SAI_GetClassicI2SConfig(&g_transceiverConfig, DEMO_AUDIO_BIT_WIDTH, kSAI_Stereo, kSAI_Channel0Mask)
to
SAI_GetClassicI2SConfig(&g_transceiverConfig, DEMO_AUDIO_BIT_WIDTH,kSAI_MonoRight, kSAI_Channel0Mask)
.But I think I miss something in config (Because the time to get buffer full is double than the original config).
1. I think I had to reconfig clock or something else...?
2. I found SAI_RxSetBitClockRate(DEMO_SAI, DEMO_AUDIO_MASTER_CLOCK, DEMO_AUDIO_SAMPLE_RATE, DEMO_AUDIO_BIT_WIDTH,
DEMO_AUDIO_DATA_CHANNEL). What is this config used for? The DEMO_AUDIO_DATA_CHANNEL means? If I record mono, then the DEMO_AUDIO_DATA_CHANNEL = 1?
Thanks in advance.
Hello,
To work in mono-right mode, you need to implement the following changes.
1. Set the DEMO_AUDIO_DATA_CHANNEL to 2.
2. Set two channels as the input of the WM8960 like this:
wm8960Config.leftInputSource = kWM8960_InputDifferentialMicInput3,
wm8960Config.rightInputSource = kWM8960_InputDifferentialMicInput2;
3. Set the kSAI_MonoRight(01), this means that we will ignore the left word.
SAI_GetClassicI2SConfig(&g_transceiverConfig, DEMO_AUDIO_BIT_WIDTH, kSAI_MonoRight, kSAI_Channel0Mask);
I already made the tests on my end, and everything worked as expected.
Regards,
Victor