Can the I2S wake up the system(RT1061) from stop mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the I2S wake up the system(RT1061) from stop mode?

469 Views
StephenYeh
Contributor III

I check the reference manual the SAI interface can wake-up from STOP mode.

Does it mean that RT1061 can receive voice to wake up my CPU from STOP mode?

Labels (1)
0 Kudos
Reply
1 Reply

462 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Stephen,

That is correct, as the reference manual states the SAI transmitter receiver can generate an asynchronous interrupt to wake the CPU from Stop mode.

Have a great day,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 Kudos
Reply