CMSIS NN library for MCUXpresso SDK 2.11

cancel
Showing results for 
Search instead for 
Did you mean: 

CMSIS NN library for MCUXpresso SDK 2.11

Jump to solution
344 Views
yf2
Contributor III

Dear support,

I noticed that the CMSIS NN library is missing in $SDK/CMSIS/ folder of v2.11 SDK.

How could I add the missing CMSIS NN library to this SDK?

It seems that the CMSIS library shipped with SDK v2.11 is close to v5.6.0 version of CMSIS on Github, but the version in SDK might already have some improvements or bugfixing.

Can we simply grab the NN library in the CMSIS v5.6.0 Github release? I am wondering why SDK owner don't do it if it is that simple.

 

Regards,

yf2

Tags (1)
0 Kudos
1 Solution
314 Views
CarlosGarabito
NXP Employee
NXP Employee

We recently update the SDK and MCUXpresso IDE, some bug was eliminated, so check it this error was clean

Have a good day

View solution in original post

0 Kudos
3 Replies
315 Views
CarlosGarabito
NXP Employee
NXP Employee

We recently update the SDK and MCUXpresso IDE, some bug was eliminated, so check it this error was clean

Have a good day

0 Kudos
312 Views
yf2
Contributor III

@CarlosGarabito 

Did you mean that SDK v2.12 has CMSIS-NN included by default?

I manually added CMSIS-NN to SDK as a sibling folder of DSP/ and Core/, so far no issues have been noitced yet.

Regards,

yf2

0 Kudos
308 Views
yf2
Contributor III

@CarlosGarabito 

I just downloaded a copy of SDK v2.12 and noticed that CMSIS/NN folder exists.

Will close this ticket.

yf2

 

Tags (1)